flash progrramer not programming memory at 0x2180

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash progrramer not programming memory at 0x2180

1,571件の閲覧回数
martinlockner
Contributor III

I am using code warrior 10.4 for the MC9S08DZ128 microcontroller. When using debug to load my code everything works fine (with the PE Micro USB multilink). If I use the built in flash programmer the memory at 0x2180 and continuing for around 100 bytes does not program. I looked through the various settings but could not find anything that would exclude this area. Anyone run into this?


ラベル(1)
0 件の賞賛
返信
0 返答(返信)