flash progrramer not programming memory at 0x2180

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flash progrramer not programming memory at 0x2180

1,617 Views
martinlockner
Contributor III

I am using code warrior 10.4 for the MC9S08DZ128 microcontroller. When using debug to load my code everything works fine (with the PE Micro USB multilink). If I use the built in flash programmer the memory at 0x2180 and continuing for around 100 bytes does not program. I looked through the various settings but could not find anything that would exclude this area. Anyone run into this?


Labels (1)
0 Kudos
Reply
0 Replies