flash progrramer not programming memory at 0x2180

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

flash progrramer not programming memory at 0x2180

1,594 次查看
martinlockner
Contributor III

I am using code warrior 10.4 for the MC9S08DZ128 microcontroller. When using debug to load my code everything works fine (with the PE Micro USB multilink). If I use the built in flash programmer the memory at 0x2180 and continuing for around 100 bytes does not program. I looked through the various settings but could not find anything that would exclude this area. Anyone run into this?


标签 (1)
0 项奖励
回复
0 回复数