cwide.exe has  stopped working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cwide.exe has  stopped working

1,595件の閲覧回数
yaakovbar-on
Contributor I

I use CodeWarrior version 10.8.3 on windows 8. I used it as simulator and has problemthat  when run the code with  trace And profile.

At the end of run appear a message "cwide.exe has  stopped working"

ラベル(1)
0 件の賞賛
返信
1 返信

1,482件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I ever had one customer met similar problem with CW.

It seems that this issue is caused by a installation problem. Or, conflicting with anti-virus would also cause such a problem.

so, may I propose a re-installing of the application from scratch? A repair install may not do the job.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信