cwide.exe has  stopped working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cwide.exe has  stopped working

1,583 Views
yaakovbar-on
Contributor I

I use CodeWarrior version 10.8.3 on windows 8. I used it as simulator and has problemthat  when run the code with  trace And profile.

At the end of run appear a message "cwide.exe has  stopped working"

Labels (1)
0 Kudos
Reply
1 Reply

1,470 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I ever had one customer met similar problem with CW.

It seems that this issue is caused by a installation problem. Or, conflicting with anti-virus would also cause such a problem.

so, may I propose a re-installing of the application from scratch? A repair install may not do the job.


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply