copy code from target

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

copy code from target

2,091 Views
JohnnyP
Contributor III

Hi to all:

I'm programming a noise cancellation algorithm on the 9s12C32 processor using Code Warrior v5.5.1272 with the True-Time Simulator and Debugger, V6.1

I started the project a few years ago, got Prototype #1 up and running, then had to set it aside for four years due to my wife's illness.

Now I am working with Prototype #2.  I programmed it with the most recent version of my algorithm.

I have both prototypes running side by side on my test bench, using the same input signal, but the output from Prototype #1 is a little cleaner.

Is there a way to read or copy the code in Prototype #1?  It's unsecured.

Would I be able to make sense of it so I can update my source code?  In the "code" column is the number 620, so I guess it uses 620 bytes?

Thanks for your help.

0 Kudos
Reply
1 Reply

2,083 Views
ZhangJennie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply