commExpert not registered!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

commExpert not registered!!

2,722件の閲覧回数
ssssss
Contributor II

hi

i have codewarrior v8.8 and netcomm . i have problem with commExpert .when i open it , it says that it is a not registered version . and whenever i want to register it through registration menu in help tab , it says that : " registration failed , check if mail is working properly and retry " .

what should i do ?

 

thanks

ラベル(1)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

2,608件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello mohammad bahari,

Which version NetComm software do you use? And which processor do you use?

I have installed GA 4.4, only QorIQ Configuration Suite Tool is available.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,608件の閲覧回数
ssssss
Contributor II

hi

i use netcome release 2.2 . my processor is mpc8306 and mpc8568 .

is your commexpert registered?

On Mon, Jul 13, 2015 at 11:30 AM, yipingwang <[email protected]>

0 件の賞賛
返信

2,608件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello mohammad bahari,

Please refer to the link NetComm Software Resources|Freescale , there is no formal release version for GA2.2.

Where did you get it?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信