codewarrior and eclipse

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

codewarrior and eclipse

3,887件の閲覧回数
Krazzyonskates
Contributor I

Does anyone know how to create a project with 10.5 for a hc12 processor other than s08 or what is available.

 

 

 

Or does anyone have a project already made for an hc12?

 

 

 

Or does someone know how to take an existing project and change it to accommodate any hc12?

 

 

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

3,416件の閲覧回数
BlackNight
NXP Employee
NXP Employee

I did that a while back:

http://mcuoneclipse.com/2012/02/13/make-my-make-with-eclipse-and-mcu10/

It works the same way (with make files) for S12/HC12, as the build tools (compiler, linker) are command line tools. Actually the command line commands are pretty much the same as for S08, so can be used the same way.

I hope this gives an idea?

If there is enough interest (and I find time), I could set up someting for S12 similar to what is describe in this series (but using S12 instead of ARM):

DIY Free Toolchain for Kinetis: Part 1 – GNU ARM Build Tools | MCU on Eclipse

Of course the compiler would not be free ;-)

0 件の賞賛
返信