codewarrior 10.6 with codewarrior 10.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

codewarrior 10.6 with codewarrior 10.4

跳至解决方案
2,004 次查看
mlockner
Contributor I

Can I have both codewarrior 10.6 and codewarrior 10.4 installed on the same computer? I have an old project that was done with 10.4 and I have the need to help on a project that was started with 10.6.

标签 (1)
0 项奖励
回复
1 解答
1,710 次查看
BlackNight
NXP Employee
NXP Employee

yes. I'm using that all the time.

I recommend that for each IDE/CW you have its own workspace, e.g.

- wsp_10.6

- wsp_10.4

so you keep the IDE settings/etc separate. Mixing workspaces with different Eclipse versions is a bad thing.

Erich

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,711 次查看
BlackNight
NXP Employee
NXP Employee

yes. I'm using that all the time.

I recommend that for each IDE/CW you have its own workspace, e.g.

- wsp_10.6

- wsp_10.4

so you keep the IDE settings/etc separate. Mixing workspaces with different Eclipse versions is a bad thing.

Erich

0 项奖励
回复