code warrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

code warrior

Jump to solution
2,697 Views
hyunuk_ha
Contributor I

OS compatibility problem : 

Code Warrior version : v2.1

OS : Windows 10 x64

I installed Code warrior ver. 2.1. on Windows 10 x64, and it can't executed on this environment. 

The error log is attached as captured image. 

Is anyone help this matter to solve?

 # codewarrior‌ crash‌ unable to launch‌ #windows10‌

1 Solution
2,610 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

Normally this error is because your CW components are not well registered.

Run file regservers.bat under your CW install folder can solve the problem.

But I am aware you use CW2.1. this version doesn't support win10 officially.

CodeWarrior® Development Tools for MPC5xx|NXP 

pastedImage_2.png

Please use CW on our recommend windows platform.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,611 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

Normally this error is because your CW components are not well registered.

Run file regservers.bat under your CW install folder can solve the problem.

But I am aware you use CW2.1. this version doesn't support win10 officially.

CodeWarrior® Development Tools for MPC5xx|NXP 

pastedImage_2.png

Please use CW on our recommend windows platform.


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------