code warrior (V10.5) can not file the head file ,but there is nothing wrong with the coding.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code warrior (V10.5) can not file the head file ,but there is nothing wrong with the coding.

2,241件の閲覧回数
andylong
Contributor I

code warrior (V10.5) can not file the head file ,but there is nothing wrong with the coding.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,129件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ANDY,

So where are these header files ?

pastedImage_1.png

please add the path to Includes paths "

pastedImage_2.png

If still can not work well ,please take a screenshot about the error , also can send the project to me .

Hope it helps

ALice

0 件の賞賛
返信

2,129件の閲覧回数
andylong
Contributor I

Thank you very much for help, But I do not know to set the including path ..?

0 件の賞賛
返信