ccs protocol plugin:reading memory failed.[cannot start SAP transaction]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ccs protocol plugin:reading memory failed.[cannot start SAP transaction]

4,142件の閲覧回数
karthikaradhya
Contributor I

In one of the PCB,i have used MPC8572 power pc.

Design is finalized and card is in production.

out of 16 no assembled cards,one card is having the above mentioned issue.

Writing is successful but reading memory failed.

Please suggest me how to troubleshoot this problem.

Plz refer attached snapshots for more info.

0 件の賞賛
返信
1 返信

3,894件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello karthik aradhya,

It seems that there is problem in DDRC INITIALIZATION section in CodeWarrior initialization file.

Do you use DDR2 on your target board?

Please refer to the attached tool to calculate DDR controller register configuration parameters.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信