cant get code warrior 6.3 to work on windows 10 64 bit...download does not load files after moving link to computer desktop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cant get code warrior 6.3 to work on windows 10 64 bit...download does not load files after moving link to computer desktop

1,286 Views
joemarsh
Contributor I

Can anybody help...Learning on the HCS12 chip this semester,.  bought a new HP LAPTOP and so far its been nothing but a challenge.

I am trying to follow a video that my teacher passed to me to download the 64 bit version by deleting some files and using the remove vbs file program, but after the 447k file for CW is downloaded, and I do not have the option to Extract it since its already an .exe file

 

What am i doing wrong? JOE

Labels (1)
0 Kudos
Reply
1 Reply

1,086 Views
TICS_Fiona
NXP Employee
NXP Employee

Hi Joe,

For HCS12 products, please select CW v5.1, it supports windows 7 and other 64 bit OS.
This version can be downloaded from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-HCS12X

Hope it helps!

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply