amd16x2.elf: "Sector Protection Error" (S29GL01GS)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

amd16x2.elf: "Sector Protection Error" (S29GL01GS)

5,576件の閲覧回数
josipvrdoljak
Contributor I

Hello,

 

we try to program NOR-Flash (2x S29GL01GS in parallel, 32-bit) using "amd16x2" algorithm.

 

"Diagnose", "Unprotect" and "Erase" procedure do working fine.

When "Programm" procedure starts the flash driver reports the following error: "Sector Protection Error" (see Attachment).

 

Regards

Josip

Original Attachment has been moved to: sector-protection-error_log.txt.zip

ラベル(1)
0 件の賞賛
返信
10 返答(返信)

5,129件の閲覧回数
josipvrdoljak
Contributor I

Hello Yiping,

have you any idea or suggestions where the problem can be?

Regards

Josip

0 件の賞賛
返信

5,129件の閲覧回数
dhanasekaran
Contributor III

Hello Josip

We are facing same problem that is "Diagnose", "Unprotect" , dump  and "Erase"  operations are works fine but can't write.

We got "sector protection error". can you suggest us any solution if you found?.

Regards,

K dhabasekaran

0 件の賞賛
返信

5,129件の閲覧回数
josipvrdoljak
Contributor I

Hello Yiping,

i do not using the P4080DS board. I do  using P3041 based board which is designed by our self.

Our flash configuration is as following:

CS#0: 32-bit (2x 16-bit S29GL01GS device)

The programming of the flash at the address 0xFFF8_0000 is working fine.

But, if i start to programm the flash at address 0xFFF0_0000 i get the error message.

If i use the "U-BOOT" software which is loaded to the address 0xFFF8_0000 and running fine to programm the flash at the address 0xFFF0_0000 it works fine. We use the same register setup as is used in our TCL-script.

Why i should change the port size to 16-bit if we have a 32-bit port size.

Regards

Josip

0 件の賞賛
返信

5,129件の閲覧回数
josipvrdoljak
Contributor I

I'm using only the "HPX3-1401_C_Debug.tcl" initialization file. 

pastedImage_1.png

pastedImage_2.png

0 件の賞賛
返信

5,129件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Josip Vrdoljak,

It seems that there is problem in eLBC_BR0 and OR0 configuration.

Configuring eLBC_BR0[PS] as "10" would be more suitable.

Please refer to eLBC_BR0[PS](19–20) configuration

Port size. Specifies the port size of this memory region. For BR0, PS is configured from the boot ROM location field in the reset configuration word as loaded during reset . For all other banks the value is reset to 00 (port size not defined).
00 Reserved
01 8-bit (supported for GPCM, UPM, FCM)
10 16-bit (supported for GPCM, UPM )
11 Reserved

Have you tried the original ELBC configuration in P4080DS initialization file.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,128件の閲覧回数
josipvrdoljak
Contributor I

Hello Yiping,

here the initialization file i'm using:

0 件の賞賛
返信

5,128件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Josip Vrdoljak,

Please check your CodeWarrior launch configuration, did you use memory configuration file?

Thanks,

Yiping

0 件の賞賛
返信

5,128件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Josip Vrdoljak,

I checked P4080DS sample project, the following memory ranges are reserved in the memory configuration file.

Please don't use memory configuration file when use CodeWarrior to connect to the target board.

Please open memory configuration panel from Run->Debug Configurations-><Project>-core00_RAM_P4080_Download->Edit->Edit->Memory, and uncheck Memory configuration.

reserved v:0xF0000000 v:0xF3FFFFFF
reserved p:0xF0000000 p:0xF3FFFFFF
reserved i:0xF0000000 i:0xF3FFFFFF

reserved v:0xF4400000 v:0xF7FFFFFF
reserved p:0xF4400000 p:0xF7FFFFFF
reserved i:0xF4400000 i:0xF7FFFFFF

reserved v:0xF8030000 v:0xFDFFFFFF
reserved p:0xF8030000 p:0xFDFFFFFF
reserved i:0xF8030000 i:0xFDFFFFFF

reserved v:0xFF000000 v:0XFFDEFFFF
reserved p:0xFF000000 p:0XFFDEFFFF
reserved i:0xFF000000 i:0XFFDEFFFF

reserved v:0xFFDF1000 v:0xFFFFEFFF
reserved p:0xFFDF1000 p:0xFFFFEFFF
reserved i:0xFFDF1000 i:0xFFFFEFFF

If your problem remains, would you please provide your CodeWarrior initialization file?

I checked P4080DS CW initialization file, ELBC memory map should be located from 0xE0000000 to 0xEFFFFFFF, did you modify the memory map for your own board?


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,128件の閲覧回数
josipvrdoljak
Contributor I

Hi Carlos,

I'm using "P3041 QorIQ" and "CodeWarrior Development Studio Version: 10.3.3 Build Id:131024"

Best Regards

Josip

0 件の賞賛
返信

5,128件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee


Hi Josip,

Could you tell us which MCU and CodeWarrior version are you using?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信