adv7482 driver:Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

adv7482 driver:Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument

4,324 Views
Ohm86
Contributor I

Hello,

I am using adv7482 driver on iMx8mPlus board. 
Please anyone can help me to solve below  issue :

Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument 
Failed to probe pixel aspect ratio with VIDIOC_CROPCAP: Invalid argument

I have attached the logs file please look into this and help me to get rid of this issues.

Thanks in advance.

0 Kudos
Reply
3 Replies

4,276 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the BSP version that you are using for your test?
Also, are you testing on the EVK?

Best regards/Saludos,
Aldo.

0 Kudos
Reply

4,255 Views
Ohm86
Contributor I

Hello AldoG,

Thanks for replying.

I am using below bsp version

mickledore imx-6.1.55

and also i have imx8Mplus development board.

gstreamer version is 1.22

0 Kudos
Reply

4,148 Views
Ohm86
Contributor I

Hello AldoG,

Any Update?? Because  I am still not able to resolve the issue.
I have same issue as mentioned below link:

https://community.nxp.com/t5/i-MX-Processors/custom-image-sensor-driver/m-p/1860270

 

0 Kudos
Reply