adv7482 driver:Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adv7482 driver:Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument

4,285件の閲覧回数
Ohm86
Contributor I

Hello,

I am using adv7482 driver on iMx8mPlus board. 
Please anyone can help me to solve below  issue :

Failed to get default crop rectangle with VIDIOC_G_SELECTION: Invalid argument 
Failed to probe pixel aspect ratio with VIDIOC_CROPCAP: Invalid argument

I have attached the logs file please look into this and help me to get rid of this issues.

Thanks in advance.

0 件の賞賛
返信
3 返答(返信)

4,237件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

Could you share the BSP version that you are using for your test?
Also, are you testing on the EVK?

Best regards/Saludos,
Aldo.

0 件の賞賛
返信

4,216件の閲覧回数
Ohm86
Contributor I

Hello AldoG,

Thanks for replying.

I am using below bsp version

mickledore imx-6.1.55

and also i have imx8Mplus development board.

gstreamer version is 1.22

0 件の賞賛
返信

4,109件の閲覧回数
Ohm86
Contributor I

Hello AldoG,

Any Update?? Because  I am still not able to resolve the issue.
I have same issue as mentioned below link:

https://community.nxp.com/t5/i-MX-Processors/custom-image-sensor-driver/m-p/1860270

 

0 件の賞賛
返信