You ready for some binary interface app?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

You ready for some binary interface app?

You ready for some binary interface app?

The great thing with CodeWarrior development Suites is that you can develop almost in any programming environment out there, even if it's assembly.

 

In this occassion, I ran into a Reference Manual regarding a StarCore ABI (Application Binary Interface)

 

This document defines a set of standards to ensure interoperability between conforming CodeWarrior for StarCore software components, such as, compilers, assemblers, linkers, debuggers, and assembly language code. These standards cover run-time aspects as well as object formats to be used by compatible tool chains from StarCore and third-party tools developers.

 

A benefit of this standard definition is interoperability of conforming tools so that users can select the best tool for each phase of the application development cycle, rather than being constrained to using an entire tool chain. Another benefit is compatibility of conforming libraries. Us programmers can build compatible binary libraries and assembly code libraries and be assured of their continued compatibility over time.

 

So if you are ready for a new experience at programming (in case binary interfaces are your thing) start along with this Reference Manual!

2096_2096.jpgbinary.jpg

 

ラベル(1)
評価なし
バージョン履歴
最終更新日:
‎09-09-2012 03:08 PM
更新者: