Writing Data to a File in CodeWarrior

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Writing Data to a File in CodeWarrior

1,544件の閲覧回数
scottgaetjens
Contributor I

Hello.  I am trying to write the data taken from the line scan camera to a file so that my team and I can look at it and plot it in excel to make sure our code is correct.  I've tried using standard libraries like stdio.h and fstream.h to do this, but CodeWarrior seems to have no clue what those are.  Below is a screenshot of my code.  Any suggestions would be greatly appreciated!

 

20871_20871.pngCapture.PNG.png

ラベル(1)
0 件の賞賛
返信
1 返信

1,372件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Please replace the MSL C library with the one that supports FileIO, the libraries should have been placed under CodeWarrior installation folder. And usually user can find such information in Compiler Manual or Build Tools Reference Manual, which are also included in CodeWarrior folder.

For details, please reply the CodeWarrior version you are using, as well as the part number of your MCU or Processor. Thanks!

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信