Windows 10 -codewarrier v 9.2 Not working.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Windows 10 -codewarrier v 9.2 Not working.

2,204 次查看
rakinniyapramod
Contributor I

I 'm trying to erase a chip using codewarrier usb tap with Codewarrier version 9.2 mobileGT. It is not working - shows an error "please check Jtag CLK speed" . 

Is this an issue with windows 10 how can this be solved?

There are reports of issues with codewarrier in windows 10. It seems to work fine with XP or 7.

The device I am using is S29GL128P. Is there any other version that will support this?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

2,065 次查看
Pavel
NXP Employee
NXP Employee

See the AN4338 about using USB TAP under Windows 7.

Try to use this Application Note for under Windows 10.

 

Use CodeWarrior TAP under Windows 10.

 

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,065 次查看
rakinniyapramod
Contributor I

Can you please provide the attachment for the document?

0 项奖励
回复