Windows 10 -codewarrier v 9.2 Not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Windows 10 -codewarrier v 9.2 Not working.

2,120 Views
rakinniyapramod
Contributor I

I 'm trying to erase a chip using codewarrier usb tap with Codewarrier version 9.2 mobileGT. It is not working - shows an error "please check Jtag CLK speed" . 

Is this an issue with windows 10 how can this be solved?

There are reports of issues with codewarrier in windows 10. It seems to work fine with XP or 7.

The device I am using is S29GL128P. Is there any other version that will support this?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,981 Views
Pavel
NXP Employee
NXP Employee

See the AN4338 about using USB TAP under Windows 7.

Try to use this Application Note for under Windows 10.

 

Use CodeWarrior TAP under Windows 10.

 

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,981 Views
rakinniyapramod
Contributor I

Can you please provide the attachment for the document?

0 Kudos
Reply