Why there are many pop-up screens which is 'PPC EABI C/C++ stop to work' when i build any projects in newly installed CW10.5/10.6?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Why there are many pop-up screens which is 'PPC EABI C/C++ stop to work' when i build any projects in newly installed CW10.5/10.6?

863 次查看
chenxing
Contributor I

Why there are many pop-up screens which is 'PPC EABI C/C++ stop to work' when i build any projects in newly installed CW10.5/10.6?

标签 (1)
0 项奖励
回复
1 回复

750 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello chen

I have seen the similar problem from our customer.  Do you have license file under the folder:  “C:\Freescale\CW MCU v10.6\MCU”?

It was a problem with the license manager as I suspected based on the faulting module LMGR11.dll reported by Windows.

The customer found a solution with Google from discussions of CodeWarrior users. The license manager crashes like this if you have files with invalid date on your computer.

In addition, v10.6 is an old version. Please upgrade to CW10.6.6.

Please first install CW10.6.4 which can be downloaded from:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP

Its update v10.6.5 and v10.6.6 are also available at the same link.

Best Regards

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复