Why program halt at void __thumb_startup(void)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Why program halt at void __thumb_startup(void)?

跳至解决方案
1,915 次查看
修華許
Contributor III

I use Kinetic FRDM-KE06Z as development board and use codewarrior

My colleague told me to unzip the exported archive to workspace.

Then use import from root to import this project.

 

It is ok at building the project and without any error message.

But when run and debug the project .

It is so easy to stop at _arm_start.c

and halt at

void __thumb_startup(void)

 

 

{

 

 

  // Setup registers

 

 

  __init_registers();                    // Stop here

...

 

 

What does that mean?

Any suggestion for me ? Thanks in advance

标签 (1)
0 项奖励
回复
1 解答
1,725 次查看
修華許
Contributor III

OK.

Sorry I think it is Watch Dog .

But I confused that I did create a watchdog component in PE.

But I chose not to initialize it

It still works.  :smileysad:

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,726 次查看
修華許
Contributor III

OK.

Sorry I think it is Watch Dog .

But I confused that I did create a watchdog component in PE.

But I chose not to initialize it

It still works.  :smileysad:

0 项奖励
回复