Why program halt at void __thumb_startup(void)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why program halt at void __thumb_startup(void)?

Jump to solution
1,901 Views
修華許
Contributor III

I use Kinetic FRDM-KE06Z as development board and use codewarrior

My colleague told me to unzip the exported archive to workspace.

Then use import from root to import this project.

 

It is ok at building the project and without any error message.

But when run and debug the project .

It is so easy to stop at _arm_start.c

and halt at

void __thumb_startup(void)

 

 

{

 

 

  // Setup registers

 

 

  __init_registers();                    // Stop here

...

 

 

What does that mean?

Any suggestion for me ? Thanks in advance

Labels (1)
0 Kudos
Reply
1 Solution
1,711 Views
修華許
Contributor III

OK.

Sorry I think it is Watch Dog .

But I confused that I did create a watchdog component in PE.

But I chose not to initialize it

It still works.  :smileysad:

View solution in original post

0 Kudos
Reply
1 Reply
1,712 Views
修華許
Contributor III

OK.

Sorry I think it is Watch Dog .

But I confused that I did create a watchdog component in PE.

But I chose not to initialize it

It still works.  :smileysad:

0 Kudos
Reply