Which version of codewarrior is required to run MQX 4.2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Which version of codewarrior is required to run MQX 4.2.0

880 次查看
sivapalana
Contributor I

Iam currently porting from mqx 4.0.2 to 4.2.0. Currently iam using  code warrior version 10.4 , I would like to know whether this suports mqx 4.2.0 or i need to download any other version of  code warrior?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

812 次查看
TICS_Fiona
NXP Employee
NXP Employee

Hello sivapalan

Freescale MQX RTOS 4.2 was compiled and tested with these development tools:

• Kinetis Development Studio version 3.0.0

• CodeWarrior Development Studio for Microcontrollers version 10.6

• IAR Embedded Workbench for ARM® Version 7.40.1

So I would recommend updating CodeWarrior to v10.6.4:

http://tinyurl.com/6jo5tge

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复