Which version of CodeWarrior has support for MSC8157?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which version of CodeWarrior has support for MSC8157?

Jump to solution
1,651 Views
yavv
Contributor I

Hello.

 

Which version of CodeWarrior has support for MSC8157 DSP's?

 

I downloaded CW 10.7.2, but it has support for PSC9x3x only.

CW 3.2.3 doesn't support MSC8157 too.

 

Where can I find CW suitable for MSC8157 development?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,589 Views
TICS_Fiona
NXP Employee
NXP Employee

User developing for the MSC8157/8 should use CodeWarrior v10.5.0 which can be downloaded from:

CodeWarrior Legacy Downloads|Freescale

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,590 Views
TICS_Fiona
NXP Employee
NXP Employee

User developing for the MSC8157/8 should use CodeWarrior v10.5.0 which can be downloaded from:

CodeWarrior Legacy Downloads|Freescale

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply