Which version of CodeWarrior has support for MSC8157?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Which version of CodeWarrior has support for MSC8157?

跳至解决方案
991 次查看
yavv
Contributor I

Hello.

 

Which version of CodeWarrior has support for MSC8157 DSP's?

 

I downloaded CW 10.7.2, but it has support for PSC9x3x only.

CW 3.2.3 doesn't support MSC8157 too.

 

Where can I find CW suitable for MSC8157 development?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
929 次查看
TICS_Fiona
NXP Employee
NXP Employee

User developing for the MSC8157/8 should use CodeWarrior v10.5.0 which can be downloaded from:

CodeWarrior Legacy Downloads|Freescale

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
930 次查看
TICS_Fiona
NXP Employee
NXP Employee

User developing for the MSC8157/8 should use CodeWarrior v10.5.0 which can be downloaded from:

CodeWarrior Legacy Downloads|Freescale

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复