Where to download hc12xd derivative?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where to download hc12xd derivative?

1,270 Views
juancarloserroa
Contributor I

I just download "CodeWarrior for HCS12(X) Microcontrollers v5.2" but it doesn't have hc12xd derivative. I tryied to find it but I didn't.

Labels (1)
0 Kudos
Reply
1 Reply

1,062 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

CW5.2 only includes support for the following derivatives. This is NXP market decision:

    - MC9S12C128, MC9S12C32, MC9S12C64, MC9S12C96

    - MC9S12G128, MC9S12G96

    - MC9S12GC128, MC9S12GC16, MC9S12GC32, MC9S12GC64

    - MC9S12GN16, MC9S12GN32

    - MC9S12P32, MC9S12P64, MC9S12P96, MC9S12P128

    - MC9S12XEP100, MC9S12XEP768

    - MC9S12XEQ384, MC9S12XEQ512

    - MC9S12XET256

    - MC9S12XS128, MC9S12XS256, MC9S12XS64

- MC9S12VR16, MC9S12VR32, MC9S12VR48, MC9S12VR64

If you want to use other hcs12(x) devices, We suggest you use CW5.1.

CW for HCS12(x) v5.1 evaluation version can be downloaded from here:

Evaluation Software|NXP

"CodeWarrior Development Studio for HCS12(X) Microcontrollers (Classic IDE) v5.1  "

CW5.1 can also support 32/64bit win7 officially without problem.

however the original install CW5.1 doesn't support some P&E tool such as Multilink FX, in this case if you want to use CW5.1 + Multilink FX, please install Patch for (S)12(X) 3rd Party Software  from P&E website:

http://www.pemicro.com/faqs/faq_view.cfm?id=211

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply