When will there be a version of the codewarrior tap probe for the mpc56xx processors?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When will there be a version of the codewarrior tap probe for the mpc56xx processors?

1,114 Views
wilhelm_von_vli
Contributor I

I want to debug my mpc5644a application while it is connected to the outside world.

This means that its placed on the other side of the building, so de codewarrior tap probe

could be a solution to controll it all by the ethernet connection.

Labels (1)
0 Kudos
Reply
1 Reply

1,046 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

CodeWarrior Tap does not support MPC56xx family and I think it will never be. But instead of it, you can use Cyclone-FX programmer, which is also debug probe. Please look at the following link:

Cyclone-FX|NXP 

Regards,

Martin

0 Kudos
Reply