When will there be a version of the codewarrior tap probe for the mpc56xx processors?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When will there be a version of the codewarrior tap probe for the mpc56xx processors?

1,117件の閲覧回数
wilhelm_von_vli
Contributor I

I want to debug my mpc5644a application while it is connected to the outside world.

This means that its placed on the other side of the building, so de codewarrior tap probe

could be a solution to controll it all by the ethernet connection.

ラベル(1)
0 件の賞賛
返信
1 返信

1,049件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

CodeWarrior Tap does not support MPC56xx family and I think it will never be. But instead of it, you can use Cyclone-FX programmer, which is also debug probe. Please look at the following link:

Cyclone-FX|NXP 

Regards,

Martin

0 件の賞賛
返信