What would it take to add MPC8xx devises into CodeWarrior Development Suites for Networked Applications v11.4.0?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What would it take to add MPC8xx devises into CodeWarrior Development Suites for Networked Applications v11.4.0?

1,548 Views
jason_maurey
Contributor I

I need to work on an older device that uses MPC8xx devices.  The website recommends CodeWarrior Development Suites for Networked Applications v11.4.0 as the software but after installation I found the MPC8xx is not supported.  I was later recommended to use CW 8.8, but CW 8.8 does not support the debuggers I have and is not playing well with windows 10. 

What would be the steps required to add MPC8xx devices into CodeWarrior Development Suites for Networked Applications v11.4.0?

Tags (1)
0 Kudos
Reply
1 Reply

1,476 Views
ufedor
NXP Employee
NXP Employee

> What would be the steps required to add MPC8xx devices into

> CodeWarrior Development Suites for Networked Applications v11.4.0?

Sorry, but this is technically impossible.

Please consider that the CodeWarrior v11.4.0 was developed and supports only ARMv8-based processors.

Please try to use the CW 8.8 under Win7 - it should work.

0 Kudos
Reply