What is the installation procedure for CodeWarrior Development Studio for StarCore 3900FP DSP v10.9.0 on a Linux host (using the IDE)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the installation procedure for CodeWarrior Development Studio for StarCore 3900FP DSP v10.9.0 on a Linux host (using the IDE)?

1,278 Views
klauffenburger
Contributor I

I downloaded the tar archive "CodeWarrior Development Studio for StarCore 3900FP DSP v10.9.0 - Linux.tgz" and extracted it to a directory, but there appears to be no IDE in the archive, and no installation instructions except for the "SC_compiler_linux_v24_07_01_013_3900.README.txt" file, which refers to this release as a patch.  Should the contents of this directory tree be somehow plugged in to an existing eclipse installation?  If so, what is the procedure for doing this?

Labels (1)
0 Kudos
Reply
1 Reply

1,235 Views
lunminliang
NXP Employee
NXP Employee

Hello Ken Lauffenburger,

No need to install, use this from command line, as describe in the readme file.

See more detail in the scc options.

By the way, you'll need license to use this.

Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply