What is"CCSProtocolPlugin:CCS:CC network timeout"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is"CCSProtocolPlugin:CCS:CC network timeout"

2,158 Views
文俊邵
Contributor I

Hi

    I use USBTAP ONCE to connect 8037 board, when I debug, the following error.21434_21434.png2015-03-26_091443.png

I use IDE Codewarrior V8.3 . My OS is  windows 7.

Labels (1)
0 Kudos
Reply
2 Replies

1,885 Views
TICS_Fiona
NXP Employee
NXP Employee

CodeWarrior 8.3 was released before Windows 7, it is not verified on Windows 7.

However, we have tested that its build tools work well on Windows 7, only debugger does not work well, below is the solution to work it around:

To support USBTAP debugging on Windows 7, user needs to install the new CCS update, please search 'AN4338' on Freescale's website (www.freescale.com), and follow the instructions in it to install the update.

In addition, we have another CodeWarrior tool for DSC, it is Eclipse CodeWarrior v10.6, this product supports Windows 7 & 8, and you may get more information of it from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,885 Views
文俊邵
Contributor I

hi ,  
  Thanks.

How  do  I   config to support USBTAP debugging  in Eclipse CodeWarrior v10.6 .

0 Kudos
Reply