What is"CCSProtocolPlugin:CCS:CC network timeout"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is"CCSProtocolPlugin:CCS:CC network timeout"

2,148件の閲覧回数
文俊邵
Contributor I

Hi

    I use USBTAP ONCE to connect 8037 board, when I debug, the following error.21434_21434.png2015-03-26_091443.png

I use IDE Codewarrior V8.3 . My OS is  windows 7.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,875件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

CodeWarrior 8.3 was released before Windows 7, it is not verified on Windows 7.

However, we have tested that its build tools work well on Windows 7, only debugger does not work well, below is the solution to work it around:

To support USBTAP debugging on Windows 7, user needs to install the new CCS update, please search 'AN4338' on Freescale's website (www.freescale.com), and follow the instructions in it to install the update.

In addition, we have another CodeWarrior tool for DSC, it is Eclipse CodeWarrior v10.6, this product supports Windows 7 & 8, and you may get more information of it from:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10

Fiona Kuang

Technical Information & Commercial Support

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,875件の閲覧回数
文俊邵
Contributor I

hi ,  
  Thanks.

How  do  I   config to support USBTAP debugging  in Eclipse CodeWarrior v10.6 .

0 件の賞賛
返信