What is more preferable IDE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is more preferable IDE?

ソリューションへジャンプ
3,966件の閲覧回数
alexandergoldin
Contributor III

What is more preferable IDE CodeWarrior or Kinetis?

ラベル(1)
1 解決策
3,757件の閲覧回数
BlackNight
NXP Employee
NXP Employee

That's a very generic question, so here is a generic answer: it all depends on your needs.

For a comparison, you might have a look at "Comparing CodeWarrior with Kinetis Design Studio | MCU on Eclipse".

But in general: Usage of Kinetis Design Studio is recommended for new projects and new Kinetis designs, as all new development goes into KDS (and Kinetis SDK).

Erich

元の投稿で解決策を見る

7 返答(返信)
3,757件の閲覧回数
alexandergoldin
Contributor III

Are there any other opinions?

3,757件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Other options are listed here:

IDEs for Kinetis MCUs|Freescale

3,757件の閲覧回数
alexandergoldin
Contributor III

OK.

3,757件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Alexander Goldin:

I guess you mean CodeWarrior for MCU and Kinetis Design Studio, correct?

Depending on your selected Kinetis device, CodeWarrior is not supporting new Kinetis parts, but if you have a legacy one then it is still an option. The next is a good comparison article by colleague Erich Styger:

Comparing CodeWarrior with Kinetis Design Studio | MCU on Eclipse

:smileyalert: Just notice that the comparison was made with KDS v1.1.1. Kinetis Design Studio has suffered some changes since then. KDS v3.0.0 has just been released yesterday:

New Kinetis Design Studio V3.0.0 available

More information can be found in the dedicated pages for each product:

Kinetis Design Studio Integrated Development |Freescale

CodeWarrior for Microcontrollers-Eclipse IDE|Freescale

And just as a final comment, you are not tied to use one of these 2 IDEs for Kinetis Development. The next link presents more third party options:

IDEs for Kinetis MCUs|Freescale


Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,757件の閲覧回数
alexandergoldin
Contributor III

Thank you, Jorge Gonzalez!

3,758件の閲覧回数
BlackNight
NXP Employee
NXP Employee

That's a very generic question, so here is a generic answer: it all depends on your needs.

For a comparison, you might have a look at "Comparing CodeWarrior with Kinetis Design Studio | MCU on Eclipse".

But in general: Usage of Kinetis Design Studio is recommended for new projects and new Kinetis designs, as all new development goes into KDS (and Kinetis SDK).

Erich

3,757件の閲覧回数
alexandergoldin
Contributor III

Thank you :smileywink: