What is Target_ID for MPC 8240/8245 using Code Warrior TAP and GDB Proxy command?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is Target_ID for MPC 8240/8245 using Code Warrior TAP and GDB Proxy command?

2,037 Views
mdavis331
Contributor I

My team and I were able to correctly initialize and communicate with the Code Warrior TAP GDB proxy. We still need some assistance with a particular instruction. Specifically:

 

mon jtag_chain <myTarget_ID>

 

Where can I locate the correct myTarget_ID for MPC 8240 and MPC 8245?

Please refer to the following link for more context on specific question (if needed):

https://community.nxp.com/message/999148?commentID=999148&et=notification.mention#comment-999148

0 Kudos
Reply
2 Replies

1,900 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Matthew Davis,

Please try to use the command "mon jtag_chain mpc8260".

In addition, please use the CCS from CodeWarrior 8.8 with Patch 8.8.6 applied.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,900 Views
mdavis331
Contributor I

Not able to verify because I can't find CodeWarrior 8.8 with Patch 8.8.6?

Where can I download this specific version?

0 Kudos
Reply