What is Target_ID for MPC 8240/8245 using Code Warrior TAP and GDB Proxy command?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is Target_ID for MPC 8240/8245 using Code Warrior TAP and GDB Proxy command?

2,005件の閲覧回数
mdavis331
Contributor I

My team and I were able to correctly initialize and communicate with the Code Warrior TAP GDB proxy. We still need some assistance with a particular instruction. Specifically:

 

mon jtag_chain <myTarget_ID>

 

Where can I locate the correct myTarget_ID for MPC 8240 and MPC 8245?

Please refer to the following link for more context on specific question (if needed):

https://community.nxp.com/message/999148?commentID=999148&et=notification.mention#comment-999148

0 件の賞賛
返信
2 返答(返信)

1,868件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Matthew Davis,

Please try to use the command "mon jtag_chain mpc8260".

In addition, please use the CCS from CodeWarrior 8.8 with Patch 8.8.6 applied.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,868件の閲覧回数
mdavis331
Contributor I

Not able to verify because I can't find CodeWarrior 8.8 with Patch 8.8.6?

Where can I download this specific version?

0 件の賞賛
返信