What Codewarrior download do I need

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What Codewarrior download do I need

ソリューションへジャンプ
2,316件の閲覧回数
c172jeff
Contributor I

Hi,

  I am a hobbyist looking to get into making a small project that uses the MC9S08JM60CLDLD ARM chip.  I have some sample code to look at.  The author of the code says it was created in CodeWarrior 6.2.  I see there are a number of downloads.  What download do I need to install (free version of the software) to attempt to compile my sample code and get it on  a chip.  I am assuming the code and data size is small.  

I would primarily be interested in buying an arm chip, creating a small program, embedding it on the chip and debugging.

I have a Segar Jlink EDU...so I assume I will have to use that somehow.  Also, what is Coldfire?  Do I need that?

Regards,

Jeff

タグ(2)
0 件の賞賛
返信
1 解決策
2,215件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jeff

 MC9S08JM60CLDLD is 8 bit chip. not ARM. to work with it, you can use CW6.3 or CW11

CW6.2 is no longer available on external site, please use CW6.3 instead

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/8-16-bit... 

If you use 64bit win7/8/10, please use CW11

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/digital-... 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,215件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jeff

 MC9S08JM60CLDLD is 8 bit chip. not ARM. to work with it, you can use CW6.3 or CW11

CW6.2 is no longer available on external site, please use CW6.3 instead

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/8-16-bit... 

If you use 64bit win7/8/10, please use CW11

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/digital-... 


Have a great day,
Jun Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------