Version S19 file during build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Version S19 file during build

1,550件の閲覧回数
vengeful
Contributor II

Hi,

 

Not sure whether this is possible, but is there a way when generating the output ".s19" file to include a version number. Currently it just takes the name of the project, then I have to rename the file and give a version number manually, this can lead to human error.

 

Using Codewarrior IDE version 5.9

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,445件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You could run a post-build step where you perform that rename with a version number.

You can execute multiple commands (see Executing Multiple Commands as Post-Build Steps in Eclipse | MCU on Eclipse).

Erich

0 件の賞賛
返信