Variables when debugging assembly code.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Variables when debugging assembly code.

2,896 Views
mansski
Contributor I

I am using CodeWarrior V10.7. I am using pure assembly language code for MC56F84763. While debugging, is there a way to watch my variables? Can I add them to the Expressions window? If yes, how exactly should I declare them? I cannot find a way for the debugger to recognize them.

Labels (1)
0 Kudos
Reply
4 Replies

2,675 Views
eduardo_viramon
NXP Employee
NXP Employee

Fiona,

I'm a motor control systems engineer for the microcontrollers division.

Today I visited Stanko's office and he mentioned this issue to me. He has not received an answer in several months.

Can you please inform us if there are any updates on this?

Eduardo V.

0 Kudos
Reply

2,675 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Stanko and Eduardo V.

I am sorry for the delay.

I just checked ENGR00381597, this issue is still pending.
I will recontact DevTech team, I will let you know as soon I get update.

Best Regards,

Jennie Zhang

0 Kudos
Reply

2,675 Views
TICS_Fiona
NXP Employee
NXP Employee

Hello Stanko

Sorry for this inconvenience you are experiencing with our tool. 

I have contacted our debugger engineer, and submit this issue as a feature request with ID: ENGR00381597.

I will reply you as soon as I get any update. 

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,675 Views
mansski
Contributor I

Hi Mrs. Kuang,

Since it’s been already a week, I wondered if there is any word from your engineers if the V10.7 Metrowerks allows us to watch our variables when the project is only in assembly language?

Thanks,

Stanko

0 Kudos
Reply