Using the P&E Micro Multilink Universal FX with CodeWarrior 5.1 for HCS12(X) ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using the P&E Micro Multilink Universal FX with CodeWarrior 5.1 for HCS12(X) ?

3,113 次查看
Jiun_Yong
Contributor III

Can I use the P&E Micro Multilink Universal FX Debug Interface with CodeWarrior 5.1 for HCS12(X)?

标签 (1)
0 项奖励
回复
3 回复数

2,217 次查看
trytohelp
NXP Employee
NXP Employee

Hi Steve,

Officially the Multilink Universal FX was introduced at MCU v10.2 version.

So previous version and classic version are not supported by default -> this is including HC12 V5.1.

However ...

Here is patch for Universal FX interface under CW5.1.

Note: The current version of unit_12z.dll is 2.78 (released 5/9/2012)

Regards

Pascal

0 项奖励
回复

2,217 次查看
Jiun_Yong
Contributor III

That works fine. Thanks very much for your help :smileycool:

For the benefit of anybody else doing this, I found copies of unit_12z.dll in both the CodeWarrarior/Prog folder in "Program Files" and in "Windows/system32" and replaced both.

0 项奖励
回复

2,217 次查看
trytohelp
NXP Employee
NXP Employee

Hi Steve,

You're welcome.

Regards

Pascal

0 项奖励
回复