Using the P&E Micro Multilink Universal FX with CodeWarrior 5.1 for HCS12(X) ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the P&E Micro Multilink Universal FX with CodeWarrior 5.1 for HCS12(X) ?

3,151件の閲覧回数
Jiun_Yong
Contributor III

Can I use the P&E Micro Multilink Universal FX Debug Interface with CodeWarrior 5.1 for HCS12(X)?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,255件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Steve,

Officially the Multilink Universal FX was introduced at MCU v10.2 version.

So previous version and classic version are not supported by default -> this is including HC12 V5.1.

However ...

Here is patch for Universal FX interface under CW5.1.

Note: The current version of unit_12z.dll is 2.78 (released 5/9/2012)

Regards

Pascal

0 件の賞賛
返信

2,255件の閲覧回数
Jiun_Yong
Contributor III

That works fine. Thanks very much for your help :smileycool:

For the benefit of anybody else doing this, I found copies of unit_12z.dll in both the CodeWarrarior/Prog folder in "Program Files" and in "Windows/system32" and replaced both.

0 件の賞賛
返信

2,255件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Steve,

You're welcome.

Regards

Pascal

0 件の賞賛
返信