Using the P&E Micro Multilink Universal FX with CodeWarrior 5.1 for HCS12(X) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using the P&E Micro Multilink Universal FX with CodeWarrior 5.1 for HCS12(X) ?

3,197 Views
Jiun_Yong
Contributor III

Can I use the P&E Micro Multilink Universal FX Debug Interface with CodeWarrior 5.1 for HCS12(X)?

Labels (1)
0 Kudos
Reply
3 Replies

2,301 Views
trytohelp
NXP Employee
NXP Employee

Hi Steve,

Officially the Multilink Universal FX was introduced at MCU v10.2 version.

So previous version and classic version are not supported by default -> this is including HC12 V5.1.

However ...

Here is patch for Universal FX interface under CW5.1.

Note: The current version of unit_12z.dll is 2.78 (released 5/9/2012)

Regards

Pascal

0 Kudos
Reply

2,301 Views
Jiun_Yong
Contributor III

That works fine. Thanks very much for your help :smileycool:

For the benefit of anybody else doing this, I found copies of unit_12z.dll in both the CodeWarrarior/Prog folder in "Program Files" and in "Windows/system32" and replaced both.

0 Kudos
Reply

2,301 Views
trytohelp
NXP Employee
NXP Employee

Hi Steve,

You're welcome.

Regards

Pascal

0 Kudos
Reply