Using exponential function in MPC5607B controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using exponential function in MPC5607B controller

3,716 次查看
kpitsupportshas
Contributor I

Hello,

As this controller supports only fixed point arithmetic, can you please let us know how to integrate exponential function in MPC5607B. We observed that exponential function uses floating point value and its return type is float or double.

 

Regards,

Srinivasan K.

标签 (1)
0 项奖励
回复
3 回复数

3,475 次查看
kpitsupportshas
Contributor I

Hello Martin,

Thanks for quick reply.

We are using Runtime.PPCEABI.VS.UC.a library and want to use exponential(e^x) function. Could you please let us know, if this library doesn't support exponential function which library supports this?

Regards,

Srinivasan K.

0 项奖励
回复

3,473 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

include  math.h to your project. Now you can use function exp. Please look at the file in the attachment, where you find description of the function (page 111-112).

Regards,

Martin

0 项奖励
回复

3,473 次查看
martin_kovar
NXP Employee
NXP Employee

Hi,

could you please write me, which library and which function you want to use?

The fact that MPC5607B does not have SPE unit does not mean, you are not able to use floating point data types. But instead of floating point instructions, software support is used and floating point instructions has to be replace by standard VLE instructions and calculation takes more time.

Regards,

Martin

0 项奖励
回复