Unable to debug using JTAG along with multilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to debug using JTAG along with multilink

2,488 Views
maddyv
Contributor I

I am using MPC567XEVBMB + MPC5674ADAT516 + SPC5674FMVY3+ PE micro multilink universal + cw 5.9.0 Eval version. Unable to debug. Getting 'Cannot Enter Background Mode" error message.

However, Trace32 provides more details.

debug port fail
JTAGID=0x1827401D
SYStem.Up error: received invalid OSR (0x000)
- does the target assert JCOMP while RESET is asserted?
- is the device censored?
error: received invalid OSR while core running (0x000)

Whether Codewarrior and PE multilink are good for powerPC???

0 Kudos
Reply
1 Reply

2,420 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, CodeWarrior and PE can be used for this device.

To double check the MCU is not censored, you can try to configure serial boot mode or external boot mode:

pastedImage_1.png

If the device is censored and internal boot mode is selected, the nexus is disabled.

In other modes, there are states when nexus is enabled but flash won't be accessible. You can still see RAM and peripherals. This state can be used for testing.

Regards,

Lukas

0 Kudos
Reply