Unable to debug using JTAG along with multilink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to debug using JTAG along with multilink

2,469件の閲覧回数
maddyv
Contributor I

I am using MPC567XEVBMB + MPC5674ADAT516 + SPC5674FMVY3+ PE micro multilink universal + cw 5.9.0 Eval version. Unable to debug. Getting 'Cannot Enter Background Mode" error message.

However, Trace32 provides more details.

debug port fail
JTAGID=0x1827401D
SYStem.Up error: received invalid OSR (0x000)
- does the target assert JCOMP while RESET is asserted?
- is the device censored?
error: received invalid OSR while core running (0x000)

Whether Codewarrior and PE multilink are good for powerPC???

0 件の賞賛
返信
1 返信

2,401件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

yes, CodeWarrior and PE can be used for this device.

To double check the MCU is not censored, you can try to configure serial boot mode or external boot mode:

pastedImage_1.png

If the device is censored and internal boot mode is selected, the nexus is disabled.

In other modes, there are states when nexus is enabled but flash won't be accessible. You can still see RAM and peripherals. This state can be used for testing.

Regards,

Lukas

0 件の賞賛
返信