USB TAP ONCE breakpoint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB TAP ONCE breakpoint

2,779 Views
Ben
Senior Contributor I

HI

Anyone know why using the USB TAP ONCE unit and setting BP instead of showing me the code at the BP marker the debugger jump to internal interrupt?

Picture attached.

I tried using PEmicro Multilink Universal instead and it run OK.

I had the same problem with 2 USB TAO units I tested (revB)

I even tried to reset the USB TAP unit according to the manual instructions, but it did not help.

TIA

Labels (1)
Tags (3)
0 Kudos
Reply
2 Replies

2,615 Views
TICS_Fiona
NXP Employee
NXP Employee

Please delete .metadata folder of workspace of CW 10.5.

Then reopen the project in CodeWarrior, and click on 'Project' menu-> Clean to remove the old object file, and then rebuild the project. Is the problem fixed?

0 Kudos
Reply

2,615 Views
Ben
Senior Contributor I

Dear Fiona,

As you found out, there is a bug with the USB TAP ONCE that cause it.

Thank you for confirming it on the S/R, it's a pity that you don't publish this fact here to prevent community users to waist time on such bug.

0 Kudos
Reply