Type of output file is necessary to load to the program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Type of output file is necessary to load to the program

1,438 Views
sujaigowda
Contributor II

Hi,

I am using CodeWarrior v8.3 for programming of DSP56807 controller with Codewarrior USB TAP ONCE debugger, I am unable to understand what type of output file is necessary to load to the program.

0 Kudos
Reply
1 Reply

1,398 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Sujai,

The CW tools can generate the *.elf file, which you can click "debug" in CW for DSP56800E tools  to download  to flash of DSP56F807.

As the following Fig, the first file Flash is elf file, the extension name is "elf".

Hope it can help you

BR

XiangJun Rong

pastedImage_1.png

0 Kudos
Reply