There is a problem in programming 56F8323 with CodeWarrior for DSC56800E v8.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

There is a problem in programming 56F8323 with CodeWarrior for DSC56800E v8.2

ソリューションへジャンプ
2,760件の閲覧回数
kavehkiyanmajd
Contributor I

Hello,

 

I have a USB Multilink Universal (PEmicro)  ,and I installed codewarrior 8.2 in win7 64bit,when I plugin the Multilink,

its appear "usb Multilink" in device manager.

when i want to program DSC(mc56f8323) with freescale 56800E Flash programmer, i Encounter with this error:"CCCSClient::ConfigChain: USB open failure".

i do that steps in the application notes number "AN4338SW". but its not any result.

What else can I try?

Thanks in advance for any help

ラベル(1)
0 件の賞賛
返信
1 解決策
2,464件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello kaveh

To debug with CodeWarrior v8.3 on Windows 7, please choose USBTAP:

USB TAP for ONCE DSC|NXP

CodeWarrior v8.3 or 56800E Flash programmer does not support Multilink Universal. To program Multilink Universal, please choose Eclipse CodeWarrior v10.7:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

Hope this helps!

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,464件の閲覧回数
khalil001
Contributor II

Hello, I am using the MC56F8006 now, and I have the same issue as you.

Have you solve this problem now?

Could I communicate with you on MC56F8006?

Could you help me?

Thank you very much!

0 件の賞賛
返信
2,465件の閲覧回数
TICS_Fiona
NXP Employee
NXP Employee

Hello kaveh

To debug with CodeWarrior v8.3 on Windows 7, please choose USBTAP:

USB TAP for ONCE DSC|NXP

CodeWarrior v8.3 or 56800E Flash programmer does not support Multilink Universal. To program Multilink Universal, please choose Eclipse CodeWarrior v10.7:

CodeWarrior for Microcontrollers-Eclipse IDE|NXP 

Hope this helps!

Best Regards

Fiona Kuang

TIC - Technical Information Center

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Mark Correct button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信