The USBTAP driver installation was not succesful

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The USBTAP driver installation was not succesful

1,322 Views
ahnjoseph
Contributor III

I did install codewarrior 10.6.3 (For s12zvm)

but I was not able to complete the installation.

 

How can i do ? 

 

 

The USBTAP driver installation was not succesful

 

146212_146212.pngpastedImage_0.png

Labels (1)
0 Kudos
Reply
1 Reply

1,212 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

so solve this problem, please

1. make sure you have windows admin right of the computer. it's important.

2. go to windows device manager, check if there is any USBTAP or other  board related device connected. if yes, remove the related hardware connection and driver

3. s12zvm doesn't use USB tap driver. if you can't install it. you can still use s12zvm with codewarrior. seperate driver can be downloaded from P&E web site:

https://www.pemicro.com/downloads/download_file.cfm?download_id=53


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply