Technical problem with cyclone programmer model U-Cyclone

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Technical problem with cyclone programmer model U-Cyclone

6,799件の閲覧回数
mustafa_tarhan
Contributor II

our customer has faced an issue while trying to add .SAP file to the cyclone as shown in the attached photo (cyclone issue) .

they tried to access the cyclone using older version of software (cyclone pro image manager )  and it appears that the internal storage of the device is 0 Kbytes as shown in the attached photo (old version software ).

So I think there is a problem with the internal storage .

what would be the problem?

タグ(1)
0 件の賞賛
返信
2 返答(返信)

6,720件の閲覧回数
johnny_pe
Contributor III

Mustafa,

The Cyclone Image Manager is an old application that worked with the Cyclone Pro and is now deprecated. You should not use it with the Cyclone Universal. Please send an email to our technical support team so we can assist you. The email address is [email protected]

Regards,
Johnny

PEMicro Support 

0 件の賞賛
返信

6,720件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Mustafa TARHAN 

Cyclone Image management utility is P&E product.

I suggest you contact PEmicro | Experts in Embedded tools for Flash Programming and Development  for this question.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信